You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Status Bar

Status Bar

A status bar located at the bottom of the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger main window displays the five following labels from left to right:

Status Bar Labels

Figure 3-24: Status Bar Labels

An icon between the Local and Controller versions allows to show any differences (for more details, Compare PLC Programs).

The space on the left of the status bar is reserved for messages.

Local Version

This label provides information about the version locally present in the KAS IDE. There are three different states:

Controller Version

This label provides information about the version present in the controller. There are three different states:

Drives state

There are three different states:

Controller State

The Controller state label lets you know if the Controller is running or stopped. There are three different states:

Connection State

The Connection label displays the Connection state between the KAS IDE and the Controller. There are five different states:

Color Codes

The Local and Controller version labels has an orange background in case of version mismatch between the IDE and the Controller. This warns you that you have to download the new version of the application.

The Local version label has a red background if the compilation fails.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™